PDSCH/PUSCH Decoder Algorithm (5G NR/5G-Advanced)
PDSCH Physical Downlink Shared Channel/PUSCH Decoder Algorithm selects the decoder algorithm to use with PDSCH and PUSCH decoding.
Default: Offset Min-Sum
Choices: Offset Min Sum, Belief Propagation
Offset Min-Sum - Specifies the layered belief propagation algorithm with offset min-sum approximation. This algorithm is faster but less accurate than Belief Propagation.
Belief Propagation - Specifies the belief-passing or message-passing algorithm. Belief Propagation is better for accuracy but very slow.
See Also