Ant. Det. Threshold (5G NR/5G-Advanced)
Ant. Det. Threshold sets the threshold for antenna detection to ignore antenna paths with too low SNR Signal-to-Noise Ratio. The average antenna power needs to be above the antenna detection threshold compared to the reference channel in order for that antenna port to be detected by the demodulator as being present in a measurement channel.
See Also