Channels (5G NR/5G-Advanced)
Channels maps one or more measurement channels to each carrier in the configuration. Because these are indexes, they start from 0 rather than 1.
Example:
![]()
CC0 = 0:4 means channels 0, 1, 2, 3 and 4 are mapped to Component Carrier 0
CC1 = 0 means channel 0 is mapped to Component Carrier 1
CC2 = 1 means channel 1 is mapped to Component Carrier 2
CC3 = 2 means channel 2 is mapped to Component Carrier 3
CC4 = 3 means channel 3 is mapped to Component Carrier 4
The checkbox to the right of the Channels field enables or disables the component carrier's channel mapping.
See Also