Time Scale Factor (5G NR/5G-Advanced)
1
0.001 to 1000
sets the value by which to scale the bandwidth and time lengths of the measured signal. This setting can be used to compensate for mis-tuned crystals or to allow demodulation of signals at a lower rate such as half rate or 1/10 rate, or for a very high bandwidth signal.
Examples
For a 1/10 rate signal, the would be 0.1
For a crystal mistuned by 5 ppm, a value of 1.000005 or 0.999995 could be used.
For a 2GHz BW signal, the would be 20 based on a 100MHz 5G NR transmission.
See Also