Inst Ch Frequency Response (5G NR/5G-Advanced)
There are two types of traces in the Trace > Data > Demod and MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. menus that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Display parameter). See About Per-Carrier Trace Types for more information.
The Ch Frequency Response shows the response of the BWP on which the physical channel (PXSCH or CSIRS or SRS) has the maximum RB allocation. If there is no channel active on the BWPs, it shows the response of the first enabled SSB.
The trace is the non-averaged Ch Frequency Response trace data for the component carrier.
When more than one carrier is defined in the Aggregation Table, "(CCn)" will appear in the title of this trace, where "n" is the number of the component carrier whose data is displayed in the trace. Select the desired component carrier number using the Configuration > Carriers > Display parameter.
For information about Ch Frequency Response, see Ch Frequency Response.
See Also