Enhancing the Measurement Speed
You can make several choices to maximize measurement speed, as shown in the following table.
|
To increase measurement speed |
|---|
|
Remove unused traces or disable trace calculations (). |
|
Reduce the number of frequency points to the minimum required or enable in order to reduce internal vector sizes. |
|
Remove unneeded markers. |
|
When averaging is used, select fast averaging.
|
|
Select only as many channels as your measurement needs (). |
Most measurement types' help text contains a topic with more information about measurement speed: .
See Also