Spectrum (Pre-5G)
Spectrum shows the frequency spectrum of the pre-demodulated Time trace data.
When averaging is Off, Spectrum and Inst Spectrum are identical, but when averaging is turned on, Spectrum will display an averaged frequency spectrum (Inst Spectrum will still show the frequency spectrum of the current measurement).
See the Spectrum trace topic in the Reference for more information.
For consistent channel power results across all traces (Summary, Spectrum, Time, etc.), set MeasSetup > ResBW > Window Type to Uniform (Rectangular).
See Also