Demod Summary Tables and ADS
To query summary table information from the 89600 VSA in ADS, use the VSA_89600_Source part and set the OutputType property to Demod Errors. See the ADS help text for the VSA_89600_Source part for more information.
The index for each summary table data result can be queried using the ListSummaryTableResults macro. Below is part of an example output of the macro for the Digital Demodulator's Syms/Errs summary table:
Summary Table Data Results for Ch1 QPSK Quadrature phase shift keying Syms/Errs (DataName = "Syms/Errs1")
Index: 0 Data result name: "EvmRms" = 0.5409367 %rms
Index: 1 Data result name: "EvmPeak" = 1.7954 %pk
Index: 2 Data result name: "EvmPeakSym" = 0
Index: 3 Data result name: "OffsetEvmRms" = *** %rms
Index: 4 Data result name: "OffsetEvmPeak" = *** %pk