About Direct Data Connectivity

Direct Data Connectivity (Option 89601101C), or User Input, allows a user to push live IQ data into the VSA software without the use of hardware or recording files. This data can be acquired from many sources, such as hardware that does not have a VSA role driver written for it, results of a simulation, data stored in a test results database, or a stream of data in an application that needs visualization or analysis performed.

See Also

89600 VSA Measurement Platform Overview