Sample Rate (Pulse)
Menu Path:
Specifies the Sample Rate (Hz) at which the Pulse Detection and Pulse Analysis are performed.
The measurement Sample Rate (Hz) and reported Bandwidth (Hz) values are both directly related to the currently selected measurement acquisition Span (Hz) setting as follows:
- Sample Rate (Hz) = 1.28 x Span (Hz)
- Bandwidth (Hz) = Span (Hz)
You can alternatively set the desired measurement Bandwidth (Hz) by setting the Span (Hz) (
), which also updates the Sample Rate (Hz) value according to the above formula.- Default value (Sample Rate): 204.8 MHz Megahertz: A unit of frequency equal to one million hertz or cycles per second.
- Default value (Span): 160 MHz