CW Frequency Offset (Pulse)

Menu Path: Analysis > Pulse Properties > Analysis > Modulation

This parameter is used for CW waveforms and is active only when CW modulation is selected. When the Continuous Wave Pulse Modulation Type is selected, set the CW Frequency Offset Automatically or Manually:

CW Frequency Offset = Automatic

For each pulse, the mean frequency is calculated and used as the reference for that pulse.

CW Frequency Offset = Manual

Allows you to manually set the modulation frequency offset (in Hz) that will be used as the reference frequency for all pulses detected as CW modulation.