Highlight Selected Pulses on Traces (Pulse)

Menu Path: Analysis > Pulse Properties > Time

When Highlight Selected Pulses on Traces is enabled, the time samples associated with each of the Selected Pulses are highlighted using sub-part specific background colors within the Acquisition Time and synchronized Amplitude, Phase and FM Frequency Modulation time trace results (as shown below for the first 4 detected pulses). Pulse highlighting includes display of the detected Pulse index value, which is also reported separately within the Pulse Table results.

For Barker modulated pulses, FM and phase highlighting shows the individual chips.  For Triangular FM modulated pulses, FM and phase highlighting shows the separate halves of the triangle.

When Highlight Selected Pulses on Traces checkbox is disabled, no pulse highlighting is included within the time trace results.