Maximum Pulse Count (Pulse)

Analysis > Pulse Properties > Time

When the Maximum Pulse Count checkbox is enabled (checked), you can specify an upper limit to the number of detected signal pulses which should be considered for inclusion within pulse analysis results. If the measured signal contains more valid pulses than the specified Max Pulse Count, only the first Max Pulse Count number of detected signal pulses will be processed and reported within the pulse analysis results.

When the Maximum Pulse Count checkbox is disabled (unchecked), the maximum number of pulses to be analyzed is limited to 10000.

If you are unable to set your desired maximum pulse count, make sure the Maximum Pulse Count checkbox is checked (enabled).