Pulse Signal Definitions
Definitions of terms used in the 89600 VSA software for pulse measurements are derived from IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org Std 181-2011. Some or all of these terms may be used throughout the pulse measurement application.