FM Error Time
Menu Path:
FM Frequency Modulation Error Time reports pulse -synchronized, measured signal, FM error samples over time in Hz. (FM Error Time = FM Meas Time - FM Ref Time).
When Time Values Are Relative To is set to First Pulse, X-axis time values are displayed relative to first detected pulse Rise Edge (s) value.
When Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to acquisition trigger event occurrence.
The Inst FM Error Time is a non-averaged version of FM Error Time.
Valid trace Format selections are:
- Real