FM Meas Time
Menu Path:
FM Frequency Modulation Meas Time reports pulse -synchronized measured signal FM samples over time in Hz.
When Time Values Are Relative To is set to First Pulse, X-axis time values are displayed relative to first detected pulse Rise Edge (s) value.
When Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to acquisition trigger event occurrence.
When Frequency Values Are is set to Relative, Y-axis frequency values are displayed relative to current 89600 VSA software's Center Frequency (Hz) value.
When Frequency Values Are is set to Absolute, Y-values are displayed as absolute frequency values.
The Inst FM Meas Time is a non-averaged version of FM Meas Time.
Valid trace Format selections are:
- Real