Phase Error Time
Menu Path:
Phase Error Time reports pulse -synchronized measured signal phase error samples over time in degree ( Phase Error Time = Phase Meas Time - Phase Ref Time).
When Time Values Are Relative To is set to First Pulse, X-axis time values are displayed relative to first detected pulse Rise Edge (s) value.
When Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to acquisition trigger event occurrence.
The Inst Phase Error Time is a non-averaged version of Phase Error Time.
Valid trace Format selections are:
- Real