Phase Meas Time
Menu Path:
Phase Meas Time reports pulse-synchronized measured signal phase samples over time in degree.
When Time Values Are Relative To is set to First Pulse, X-axis time values are displayed relative to first detected pulse Rise Edge (s) value.
When Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to acquisition trigger event occurrence.
When Compensate Phase Results for Frequency Offset is enabled, the reported per pulse measured and reference synchronized phase trace results are automatically compensated for each specific pulse's measured mean frequency offset from the current 89600 VSA software's Center Frequency value.
The Inst Phase Meas Time is a non-averaged version of Phase Meas Time.
Valid trace Format selections are:
- Real