Phase Ref Time
Menu Path:
Phase Ref Time reports pulse -synchronized reference signal, unwrapped-phase samples over time in degree.
When Time Values Are Relative To is set to First Pulse, X-axis time values are displayed relative to first detected pulse Rise Edge (s) value.
When Time Values Are Relative To is set to Trigger, X-axis time values are displayed relative to acquisition trigger event occurrence.
When Compensate Phase Results for Frequency Offset is enabled, the reported per pulse measured and reference synchronized phase trace results are automatically compensated for each specific pulse's measured mean frequency offset from the current VSA Center Frequency value.
Valid trace Format selections are:
- Real