OFDM Err Vect Time (6GR)

The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.

The OFDM Err Vect Time trace is the time-domain counterpart to OFDM Err Vect Spectrum: per-subcarrier EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. plotted across the measurement interval (all subcarrier types), with an overlaid RMS average symbol EVM trace per symbol. Useful for spotting EVM that varies over time or symbols rather than over frequency — for example, a transient or a problem at a specific symbol position.

OFDM Err Vect Time trace

See Also

OFDM Err Vect Spectrum

OFDM RMS Error Vector Time

Available Trace Data