PDCCH MIMO Info (6GR)
The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.
The trace has the same shape as DMRS MIMO Info, but reports the PDCCH's reference-signal-based MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. results specifically: despread EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format., per-path power, time alignment error, and frequency/phase offset per port.
This trace is not averaged.
See Also