OFDM RMS Error Vector Spectrum (6GR)
The traces in the CCn and Selected Display CC menus are identical and show the same CC0 information.
The trace is the averaged counterpart to OFDM Err Vect Spectrum: per-subcarrier EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. RMS-combined across acquisitions. It differs meaningfully from the single-acquisition version only when averaging is enabled.
See Also