Frame Structure (RFID)
The trace is a table of the burst frame structure. Frame structures differ from standard to standard and multiple frame formats are defined in some standards.
The trace provides the following:
-
Link defines the direction of the burst: forward or reverse.
-
Standard displays the standard being used for the measurement.
EPCglobal C1Gen2 is the only standard supported.
-
OffIntvl (Off Interval)is the interval between bursts preceding the numbered burst. For burst #0, the table displays a set of dashes for the Off Interval value because there is no preceding burst.
-
Frame Type describes the type of frame. Additional information specific to the frame type is displayed with each frame type.
See Also