Correction (RFID)
The trace is derived by the VSA from the calibration data. The calibration data is applied to the acquired data to compensate for phase and magnitude anomalies in the VSA's hardware and software signal processing.
See Also
The trace is derived by the VSA from the calibration data. The calibration data is applied to the acquired data to compensate for phase and magnitude anomalies in the VSA's hardware and software signal processing.
See Also
|
Copyright © 2000-2026 Keysight Technologies, Inc. |