Save Options Dialog Box
Sharing Data With Other Applications
The
dialog box provides additional file options when saving traces or recordings. For all file formats except SDF, the dialog box opens when you click from the save dialog box.The list of available
properties may include the following properties depending on the data type being saved:-
data header information with the recording.
- Saves the- Does not save the data header information.
-
- The recording data is saved at the current center frequency and span settings.
- The recording data is saved at the center frequency and span at the time the recording was made.
-
- Saves only the data between the specified, Recording Properties, Playback and settings ( ).
Be aware that the data may be slightly less than specified if calibration is enabled or if the span is not a cardinal span.
- Saves the entire recording length.
See Also
Saving a Recording (Reference Recording book)