Connect
This is a Data Header variable.
Type = Short
indicates the way trace points are shown (applies to AM Amplitude Modulation - CW modulation using amplitude variation in proportion to the amplitude of the modulating signal. Usually taken as DSB-LC for commercial broadcast transmissions and DSB-SC for multiplexed systems./AM, AM/PM, and Gain Compression Graph traces).
- 0 = lines connecting points
- 1 = points shown as regular size dots
- 2 = points shown as small dots (pixels)