DemodLTECodeLength
This is a Data Header variable.
Type = Integer
DemodLTECodeLength indicates the number of bits of information contained in each Y value for the CW 0/1 Decoded Symbol Table (downlink) and the Decoded Symbol Table (uplink).
There is one Y value for every eight bits in the symbol table data. Some channel payload lengths are not a multiple of eight so the last Y value for a payload may represent less than eight bits of data.