DemodLTENoVerticalLine
This is a Data Header variable.
Type = Boolean
DemodLTENoVerticalLine specifies whether vertical lines are drawn through points for each X-axis value in the LTE trace. This data header is only applicable to the LTE trace.
"TRUE": No vertical line between points (as in the trace)
"FALSE": Vertical lines are drawn between points (as in the trace)