DemodLTERBSlotTraces
This is a Data Header variable.
Type = Boolean
DemodLTERBSlotTraces is set to TRUE if the OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. trace is plotted against RBs and slots instead of subcarriers and symbols. Otherwise, this variable is either unset or set to FALSE.