DemodSlotStartIndex
This is a Data Header variable.
Type = Array of numbers
DemodSlotStartIndex is an array of floating-point values. The data is arranged in pairs of values. For each pair of values, the first value indicates the starting time of a “slot,” and the second value indicates the ending time of the “slot.” The time values are in units of seconds.
What constitutes a "slot" depends on the measurement that is being performed. For example, in a TD-SCDMA measurement, these "slots" are the TD-SCDMA timeslots. In an RFID measurement, the "slots" are the detected RFID bursts.