DemodSymStat
This is a Data Header variable.
Type = Short
DemodSymStat array has one element per symbol, which is be used to indicate special symbols, as follows:
- 0 = unused, “ ”
- 1 = normal symbol
- 2 = Pilot, “P”
- 4 = Tri-State, “-“
- 256 = invalid symbol, “x”
- 512 = SOF symbol, “S”
- 1024 = EOF symbol, “E”
- 2048 = Delimiter symbol, “D”
- 4096 = RTCal symbol, “R”
- 8192 = TRCal symbol, “T”