DemodSyncLength
This is a Data Header variable.
Type = Short
On the symbol table data, DemodSynLength is the length in symbols of the "sync" region, which is highlighted.
This is a Data Header variable.
Type = Short
On the symbol table data, DemodSynLength is the length in symbols of the "sync" region, which is highlighted.
|
Copyright © 2000-2026 Keysight Technologies, Inc. |