Lim*Display
This is a Data Header variable.
Type = Short
In Limit Lines, Lim*Display indicates which lines (limit, margin or both) to display.
The values for Lim*Display are:
- 1 = Limit
- 2 = Margin
- 3 = Both
The '*' in Lim*Display indicates the limit line number, the first limit line being 1 (i.e. Lim1Display, Lim2Display and so on).