InputRange
This is a Data Header variable.
Type = Double
InputRange indicates the input hardware range setting for the data in Volts peak. This data header is used only when the VSA is configured for one channel.
For multiple-channel signals, InputRange1, InputRange2, InputRange3, and InputRange4 are used to indicate the hardware range setting for each channel.