InputSpan
This is a Data Header variable.
For files you save from another application and want to recall into an 89600 VSA, you can specify an input span and a sample rate (by specifying Xdelta). If the ratio of the two is not 1.28 (zoomed) or 2.56 (baseband), the VSA resamples the data.