IQ
This is a Data Header variable.
Type = Boolean
IQ is set to TRUE in the header of a recording when the recording is performed with Input Channel configuration set to I+jQ.
This is a Data Header variable.
Type = Boolean
IQ is set to TRUE in the header of a recording when the recording is performed with Input Channel configuration set to I+jQ.
|
Copyright © 2000-2026 Keysight Technologies, Inc. |