Lim*Connect
This is a Data Header variable.
Type = Boolean Array
Lim*Connect indicates whether a point is connected to the previous point. This array is the same size as the Lim*X and Lim*Y arrays.
The '*' in Lim*Connect indicates the limit line number, the first limit line being 1 (i.e. Lim1Connect, Lim2Connect and so on).