Lim*Draw
This is a Data Header variable.
Type = Short
In Limit Lines, Lim*Draw indicates how to draw between the limit points (one line or connected points).
The values for Lim*Draw are:
- 0 = One Line
- 1 = Connected Points
The '*' in Lim*Draw indicates the limit line number, the first limit line being 1 (i.e. Lim1Draw, Lim2Draw and so on).