Lim*Fail
This is a Data Header variable.
Type = Short
In Limit Lines, Lim*Fail indicates how to show the trace if the limit fails (in trace color or in fail color).
The values for Lim*Fail are:
- 0= Trace Color
- 1 = Fail Color
The '*' in Lim*Fail indicates the limit line number, the first limit line being 1 (i.e. Lim1Fail, Lim2Fail and so on).