Lim*TstLimCount
This is a Data Header variable.
Type = Short
This is the number of composite limit result lines in the Limit Line. There can be up to 4 composite limit result lines: an upper limit line, an upper margin line, a lower limit line, and a lower margin line.
The '*' in Lim*TstLimCount indicates the limit line number, the first limit line being 1 (i.e. Lim1TstLimCount, Lim2TstLimCount and so on).