Lim*XDomain
This is a Data Header variable.
Type = Short
In Limit Lines, Lim*XDomain indicates the X Domain (time or frequency) of the limit line points.
The values for Lim*XDomain are:
- 0 = Time
- 1 = Frequency
The '*' in Lim*XDomain indicates the limit line number, the first limit line being 1 (i.e. Lim1XDomain, Lim2XDomain and so on).