Lim*XRef
This is a Data Header variable.
Type = Short
In Limit Lines, Lim*XRef indicates the X Reference of the limit line points.
The values for Lim*XRef are:
- 0 = Absolute
- 1 = Relative to Center (time) or Relative to Start (frequency)
The '*' in Lim*XRef indicates the limit line number, the first limit line being 1 (i.e. Lim1XRef, Lim2XRef and so on).