Lim*YFormat
This is a Data Header variable.
Type = Short
In Limit Lines, Lim*YFormat indicates the Y Format (linear or log) of the limit line points.
The values for Lim*YFormat are:
- 0 = Linear
- 1 = Log
The '*' in Lim*YFormat indicates the limit line number, the first limit line being 1 (i.e. Lim1YFormat, Lim2YFormat and so on).