Lim*YRef
This is a Data Header variable.
Type = Short
In Limit Lines, Lim*YRef indicates the Y Reference (absolute, relative to reference level, relative to user reference or relative to trace reference) of the limit line points.
The values for Lim*YRef are:
- 0 = Absolute
- 1 = Relative to Reference Level
- 2 = Relative to User Reference
- 3 = Relative to Trace Reference
The '*' in Lim*YRef indicates the limit line number, the first limit line being 1 (i.e. Lim1YRef, Lim2YRef and so on).