Lim*YSide
This is a Data Header variable.
Type = Short
In Limit Lines, Lim*YSide indicates the side of the limit lint (upper or lower).
The values for Lim*YSide are:
- 0 = Upper
- 1 = Lower
The '*' in Lim*YSide indicates the limit line number, the first limit line being 1 (i.e. Lim1YSide, Lim2YSide and so on).