Lim*YUnit
This is a Data Header variable.
Type = Short
In Limit Lines, Lim*YUnit indicates the unit type of the Ypoints (auto, peak,RMS, power or mRMS).
The values for Lim*YUnit are:
- 0 = Auto
- 1 = Peak
- 2 = RMS
- 3 = Power
- 4 = mRMS
The '*' in Lim*YUnit indicates the limit line number, the first limit line being 1 (i.e. Lim1YUnit, Lim2YUnit and so on).