LogicalChanNum
This is a Data Header variable.
Type = Short
LogicalChanNum indicates the logical measurement channel (as opposed to the physical input channel). For example when using I+jQ (C1+j*C2) the logical channel number is 1, but it is made by combining the data from two physical inputs.