NoiseProfileY
This is a Data Header variable.
Type = Array of numbers
NoiseProfileY has units of volts squared and is assumed that the input impedance is the same as what is used for the time domain data in the file.
NoiseProfile data header keys apply when making a recording, playback, and recording export/recall for noise corrections with time domain based inputs for power spectrum or IQ-NC based measurements.