PdfRangeError
This is a Data Header variable.
Type = Boolean
If PdfRangeError is true, the internal CCDF Complementary Cumulative Distribution Function histogram overflowed. This can happen only if the signal RMS level changes drastically during the measurement.
This variable applies only for CCDF traces.