About Sharing Data
Sharing Data With Other Applications
There are several ways to share data between the 89600 VSA and other applications:
- Waveform & Signal Recordings: Saving and Recalling Recordings
- Direct Data Streaming (without hardware): Direct Data Connectivity
- Traces: Saving and Recalling Traces and Copying and Pasting Traces
- Data Registers: Using Data Registers
- ADS Software: Using the ADS interface
- .NET API 1) Access Preamble Indicator, or 2) Application Programming Interface: Using Macros or standalone .NET programs.
See Also